AnsweredAssumed Answered

our design using  ADV7619

Question asked by Kou on Feb 7, 2014
Latest reply on Feb 27, 2014 by Kaos

Dear Sir/Madam,

 

Pls refer to the attached file.

The chart shows our new design and are going to use ADV7611.

 

We have some questions about ADV7619.

 

Q1.ADV7619 provides two HDMI 1.4 inputs.

We understand that ADV7611 does not support two simultaneous HDMI inputs.

Is our understanding correct?.

 

Q2.Can one port of ADV7611 accept an input signal like and ?.

①        and shows half image of 4K2K60p,data rate is 3Gbps.

 

Q3.ADV7619 supports the following format and pixel configuration.( ADV7619_SW_Manual_Rev0.)

     SDR RGB 2 x 24bit interleaved mode

SDR 4:2:2 2 x 16bit interleaved mode

SDR 4:2:2 2 x 20bit interleaved mode

SDR 4:2:2 2 x 24bit  interleaved mode

 

     We would like to confirm the interleaved output for 3G.

     ex. The chart shows the case of (2 x 24Bit).

interleaved output:

           ->Odd dot out :24Bit

   ->Even dot out :24Bit

->Each interleave output is 960 x 2160.

 

Does ADV7611 work like this chart?.

Is our understanding correct?.

 

It would be greatly appreciated if advice could be gotten.

Sincerely yours,

Kou

Attachments

Outcomes