AnsweredAssumed Answered

ADV7391 output drive current tolerance

Question asked by ETT Employee on Feb 5, 2014
Latest reply on Mar 2, 2014 by PaulS

In the analog output specifications section of the ADV7391 datasheet, the Full-Drive Output Current has a large range (> +/-5%). Is this variance the output current produced for an input code of 255? Is there a spec for the variation when only temperature is factored in (i.e. the variance which cannot be calibrated out)? There appears to be no specification for low-drive output current min and max in the datasheet; are these numbers available elsewhere?

Outcomes