AnsweredAssumed Answered

ADV7125 questions...85C performance, 3.3V supply, and longevity

Question asked by jamaalcharles on Feb 5, 2014
Latest reply on Feb 7, 2014 by jamaalcharles

Hello,

 

We are considering using the ADV7125BCPZ170, but we have a few questions that aren't clear in the datasheet.

 

First, the datasheet states “5V SUPPLY ONLY UP TO 140MHZ AT +85DEGC”.  At3.3V OR 5V, the device has been specified for at Tmax of +85C at 140MHz.  If one uses the 240MHz or 330MHz device, then Tmax is specified to be 70degC.   What I need to verify if the 170MHz device work at 85C (at 170MHz) and with a 3.3V input?

                               

Second, again, just need to verify we can use 3.3V and 170MHz as datasheet indicates.

 

Finally, can you tell us the projected longevity for each package, LFCSP, LQFP?  

 

Thanks for your help

Outcomes