AnsweredAssumed Answered

AD7767 reflow lead free soldering possible?

Question asked by Alexxx on Jan 30, 2014
Latest reply on Feb 3, 2014 by Alexxx

Hi,

 

In data sheet of AD7767 on page 9(pdf) / 8 (footer) "absolute maximum ratings"(!) for solder temperature

there is only written vapor phase 215°C and infrared 15 sec. 220°C. No information on reflow soldering maximum temperature and time.

In contrast, the AD7195 is rated "Reflow 260°C".

 

Can I assume that with reflow soldering standard temperatures of 260°C  do no harm (that is no degradation of parameters)?

Or must I solder this device with leaded solder at max 220°C?

Outcomes