AnsweredAssumed Answered

ADV7441A EIA-343 standard

Question asked by daisu on Jan 30, 2014
Latest reply on Feb 2, 2014 by daisu

Hello,

 

We set register settings through I2C based on the script of evaluation board/
Settings are Primary Mode = 0x02、Video Standard = 0x05.
When We input SVGA  (1280x1024 @60) to ADV7441A from PC , pixel output can be done.
But, when we input Video of EIA-343A standard to ADV7441A, pixel output can not be done.

 

Question
Please let me know settings which pixel output can be done in the case of input EIA-343A standard.
Detail of EIA-343A  is below
  Horizontal frequency : 64.002 KHz±1%
  Vertical frequency :60.608 Hz±1%  
  G video signal level : 0.5~2.0V
  Sync signal level : 0.143~0.572V
  R/B video signal level : 0.4~1.6V

 

Please give me some advice if you do not mind.

Regards,

Outcomes