AnsweredAssumed Answered

ADXL345 Interfaced to Raspberry Pi

Question asked by Peetah on Jan 29, 2014
Latest reply on Feb 14, 2014 by Peetah

Hello,

I'm trying to interface the ADXL345 to my Raspberry Pi following the worked example I've got to the point where I need to download and install the patches. I have them downloaded however the command isn't recognised. Also as I don't have another Linux machine available I figured it would be easiest to do it all on the target (pi) itself and not on an external machine.

 

pi@raspberrypi ~/RaspberryPi $ git am 0001-input-adxl34x-quick-hack-for-BCM2807-which-doesn-t-s.patch
fatal: Not a git repository (or any of the parent directories): .git

 

I understand there is a linux patch command however it asks for a original file which is being patched and I don't know which that is.

 

Thanks in advance, Peter

Outcomes