AnsweredAssumed Answered

adv7511 reference design

Question asked by hsaeed on Jan 27, 2014
Latest reply on Jan 28, 2014 by DragosB

Hello All
I hope there will be some one who can help me in solving this problem.

 

When i run the reference design

http://wiki.analog.com/resources/fpga/xilinx/kc705/adv7511

on ZEDBoard from SDK.

I see the following output on terateam.

 

 

********************************************************************
ADI HDMI Trasmitter Application Ver R1.1.1
HDMI-TX: ADV7511 Rev 0x14
Created: Jan 24 2014 At 17:39:03
********************************************************************

To change the video resolution press:
'0' - 640x480; '1' - 800x600; '2' - 1024x768; '3' - 1280x720
'4' - 1360x768; '5' - 1600x900; '6' - 1920x1080.
Mute audio and video.
APP: Driver Enabled
HPD changed to HI
MSEN changed to LOW
A new EDID segment was read.
DVI device.
------------------------- EDID BLOCK 0 -------------------------
Edid Version 1.3
Mon Timing:
Pixel clock = 108.0 MHz
H Active = 1280
V Active = 1024
Progressive
No stereo
Separate sync = 3
+ve VSync
+ve HSync
Mon Freq:
Min V Freq = 56 Hz
Max V Freq = 85 Hz
Min H Freq = 30 KHz
Max H Freq = 81 KHz
Mon Name: 170T Digital

Mon Serial: H4URA09215

Edid extensions blocks: 0
########################### EDID END ###########################

 

and when i switch on and off the LCD it display the following lines in terateam.

 

MSEN changed to HI
APP: Changed system mode to Transmitter
Un-mute audio and video.
MSEN changed to LOW
APP: Changed system mode to Disconnected
Mute audio and video.

 

can any one kindly suggest me what does it mean?

how can i see some image or video?

Thanks in advance.

 

 

Regards
Hamid

Outcomes