AnsweredAssumed Answered

Alternative for AD8302

Question asked by Uda on Jan 24, 2014
Latest reply on Jan 24, 2014 by jdobler

Currently I am using a AD8302 to measure the phase  difference between two 1 GHz sinusoidal signals.  However, its Small  Signal Envelop Bandwidth is from DC to 30 MHz. I want to increase my  sampling rate to 80 Ms/s. Do you have an alternative Phase Detector with    Signal Envelop Bandwidth is grater than 80 MHz. It would also nice if  you have a  Phase Detector with a digital out put. My requirements are 1  GHZ input and 80 Ms/s.

Outcomes