AnsweredAssumed Answered

Query about ADRF6755 EVB with SDP-S and SDP-B

Question asked by WayneQ on Jan 24, 2014
Latest reply on Jan 28, 2014 by WayneQ

Hi, there

 

Please advise if this item can support SDP-S and SDP-B?

As per the CD, it only consist of the SDP-B.

How about SDP-S? And which is the program to run EVAL-ADRF6755?

 

Please also advise the following:

  • EVAL-ADRF6755 power on 5V, connected SDP-S with USB

 

  • EVAL-ADRF6755 ,inside the Regulator will shown 3.3v , it seems like only working on Regulator

 

-> EVAL-ADRF6755, PLL and other register will running only through the SDP-S with SPI is not controlling at this moment


Thanks!

 

Br,

Wayne

Outcomes