AnsweredAssumed Answered

FMCOMMS2 plugin question

Question asked by Melv_91 on Jan 21, 2014
Latest reply on Jan 21, 2014 by mhennerich

Hello Engineers,

 

In the FMCOMMS2 plugin in Linux, running at a ZC706, it is possible to load some .txt files and fed them to the DAC Buffer Output of the AD9361. I would like to read the same .txt files (such as qam16_20M.txt) with script commands. Could someone tell me how the .txt files from the plugin are fed onto the DAC output please?

In other words, how can I put the .txt files into the DAC by script commands?

 

Many thanks in advance!

 

Melv_91

Outcomes