AnsweredAssumed Answered

BF592 EZ KIT LITE PORTS PPI1Dx PPI0Dx

Question asked by KPS on Jan 20, 2014
Latest reply on Jan 23, 2014 by KPS

Hello,

 

im working with the bf592 ez kit lite.

 

I saw that in the schematics of the manual, that there are two kinds of PPI- Ports.

The PPI0Dx- and the PPI1Dx -Ports.

 

But i cant find the PPI1Dx- Ports and how to use them, in the hardware manuals.

Can someone tell me where i can find them and if its posible to use that PINs as GPIO's?

And which is the best way to use them?

 

To my project. Im evolving an Signal- generator with an simple LCD- display which is suposed to show the menue etc.

I have to use the PPI1Dx- Ports (connector P6 PIN: 52, 44, 43, 46, 45, 48, 47, 50, 49, 51, 54, 53) to control that display.

 

I hope someone can help me with that problem.

Outcomes