AnsweredAssumed Answered

Query on ADV7611 and ADV7511 video standard support

Question asked by sharathkbhat on Jan 20, 2014
Latest reply on Jan 23, 2014 by sharathkbhat

Dear Sir,

 

We are using ADV7611 and ADV7511 in our design. We wanted to check if it supports all the standards that we need. After going through  the UG and Datasheets we are able to confirm the support on few of the standards. We would like to know if the remaining standards are supported  which are not explicitly mentioned in the documentation.

 

Following is the list of standards for which we would like to know the device support,

 

ADV7611 Video Standard Support,

 

Width x Height,  Frame rate (fps), Pixel Clock (MHz)
1280 x 800,  60,  83
1280 x 800,  60, 72 Reduced Blanking
1366 x 768, 60, 85
1366 x 768,  60, 72 Reduced Blanking
1440 x 900,  60, 106
1440 x 900,  60, 88 Reduced Blanking
1600 x  900,  60, 108 Reduced Blanking
1600 x 1200,  60, 162
1680 x 1050,  60,  146
1680 x 1050,  60, 119 Reduced Blanking
1920 x 1200,  60, 154 Reduced Blanking


ADV7511 Video Standard Support,

 

Width x Height, Frame rate (fps), Pixel Clock (MHz)
800 x 600,  60,   40
1024 x 768,  60,   65
1280  x 800,  60,   83
1280  x 800,  60,  72 Reduced Blanking
1366  x 768,  60,   85
1366  x 768,  60,   72 Reduced Blanking
1440  x 900,  60,   106
1440  x 900,  60,   88 Reduced Blanking
1600  x 900,  60,   108 Reduced Blanking
1600  x 1200,  60,   162
1680  x 1050,  60,   146
1680  x 1050,  60,   119 Reduced Blanking
1920  x 1200,  60,   154 Reduced Blanking

 

Thank You,

Outcomes