AnsweredAssumed Answered

ADV7612 max current consumption with one input

Question asked by kermes on Jan 20, 2014
Latest reply on Jan 24, 2014 by kermes

Hi,

 

The power consumption in the datasheet Rev D is measured with dual 1080p 36-bit deep color with background port active.

 

Also the I(DVDDIO) typical value of 9.9mA is not sane, if maximum is 178.5mA, is this a typo?

 

I'd like to know how much is the power consumption is when there is nothing connected on the second input and it is not activated in any way.

 

A big-enough safe budgetary value for 3.3V would be fine, I don't need actual maximum.

 

Can I just halve the maximum current values of the two 3.3V nodes, I(DVDDIO) and I(TVDD) ?

 

- K

Outcomes