AnsweredAssumed Answered

AD9958 internal reference clock with 25MHz Crystal

Question asked by jonasz on Jan 17, 2014
Latest reply on Jan 19, 2014 by LouijieC

Hey,

 

I am using an AD9958 DDS on its evaluation board and tried to replace the external frequency reference source (25MHz) with an onboard crystal I bought (http://de.farnell.com/abracon/abls-25-000mhz-b2f-t/quarz-25m-18pf-cl-hc49-4hsmx/dp/1611791) which is also 25MHz.

I followed the guidance of the evaluation board and put 0Ohm resistors on positions R52 and R53 as well as 33pF capacitors on C66 and C67. Later I added in parallel 6.8pF capacitors to get closer to the desired 39pF.

Additionally I soldered 0Ohm Resistors to positions R44 to R49.

 

While the DDS works fine with jumper W11 set on external reference clock, it does not when I try to use the supplied crystal. The clock signal was monitored on J13 (SYNC CLK) and with the crystal no signal could be observed.

What am I doing wrong?


Regards,

Jonas

Outcomes