AnsweredAssumed Answered

ADV7842 Settings

Question asked by Glenn on Jan 16, 2014
Latest reply on Jan 16, 2014 by mattp

I have been using the examples in the file ADV7842-VER.5.9c_AVEB.txt (from the eval board) to set up the ADV7842 on our custom board.  This has gone well, however there is a resolution (RGB 1280x800 @ 60Hz) that we need to support that is not given as an example and is not part of the VID_STD register.  Are there example settings available for this resolution?  If not could I get some assistance with the registers (DE_H_START, etc.) that I will need to set properly for this resolution while using auto-graphics mode?

Outcomes