AnsweredAssumed Answered

VisualDSP++ conguration project fo flashing via U-Boot.

Question asked by Maksim on Jan 15, 2014
Latest reply on Jan 17, 2014 by Maksim

Hello !

I’m use BF537 EZ Lite kit. U-Boot is loaded in FLASH memory (0x20000000-0x20040000) BF537.

           How to configure Visual DSP++ (v.5.0.10) project to be loaded in FLASH memory via U-Boot ?

 

            Thank You !

         

            PS: at the moment the project is configured to boot from the UART in internal RAM.

            Load Options:   Boot Mode -> UART; Boot Format -> Intel Hex; Output Width->8-bit. ("Use default start adress" and "Verbose"           set).

            LDF setting: My program will start running from Internal memory (L1).

 

 

 

 

Outcomes