AnsweredAssumed Answered

AD9650 DCS at low Frequency

Question asked by Jaysxx on Jan 14, 2014
Latest reply on Feb 27, 2014 by Jaysxx

Setup: AD9650-80  running with input clock rate of 100 MHz and Divide-by-8 enabled (Conversion rate of 12.5 MHz).

Will DCS loop function when for this setup?

I see that the datasheet mentions DCS doesn't function for clock rates < 20 MHz. Is that for input clock rate or conversion clock rate?

Thanks.

Outcomes