AnsweredAssumed Answered

AD9467-FMC-250EBZ Clock settings

Question asked by doss on Jan 14, 2014
Latest reply on Jan 14, 2014 by doss

I can not use your design examples, because I have the SP601.

 

The clock is not very clear.

On the board is an oscilator 250Mhz.

This signal goes to AD9517-4.

 

What is the typial setting AD9517-4? I am not familar with the PLL. The datsheet is not very clear.

Can you post a typical setup for AD9517-4.

 

 

 

 

 

 

PS:  LED CR701 it extremly hot.

12V-2V/249R=40mA

LNJ314GR8TRA absolute Maximum rating 15mA!!!!!!

Outcomes