AnsweredAssumed Answered

about Absolute maximum rating AD202KY

Question asked by DMN on Jan 14, 2014
Latest reply on Jan 22, 2014 by DMN

Dear all,

 

My customer has planned the product which used AD202KY currently.

 

Their circuit is also isolated so that AD202KY may be so.

Even the GND plain has separated their circuit.

 

However, they have uneasiness.

That is because absolute maximum rating is not specified into the data sheet of AD202KY.

In their system, even when 15VDC is not supplied, input (IN+/-) voltage is applied.

 

When they use AD202KY, should it be careful of what?

And when 15VDC is not supplied, are there any clear conditions which break AD202KY?

 

Best Regards,

Fukutomi

Avnet

Outcomes