AnsweredAssumed Answered

Can AD8475 configured to a gain other than 0.4 & 0.8 using external resistors

Question asked by jebaspaul on Jan 12, 2014
Latest reply on Jan 14, 2014 by NeilJ
Branched to a new discussion

Hi,

 

I am working on multi-channel DAS. I am using AD7982 in the signal line. The dynamic range of this ADC is 5V p-p differential with a reference of +5V. The receiving signal dynamic range is 20V p-p. In a application circuit given in the datasheet of AD8475, it is used to drive AD7982. But AD8475 with a gain of 0.4 the signal dynamic range is attenuated to 4V p-p. So, I am loosing a dynamic range of 1V. So, I am thinking of using external resistors to configure AD8475 to give a gain of 0.25. I can choose the values of resistors easily. But how to select the proper resistor which has similar drift coefficients of these internal resistors used.

 

Please suggest on this.

 

Thanks,

Jebas. 

Outcomes