AnsweredAssumed Answered

Positive Gain Error correction in AD7734

Question asked by jebaspaul on Jan 7, 2014
Latest reply on Jan 16, 2014 by jebaspaul

Hi,

 

I need some clarifications with respect to the information given in the data-sheet of AD7734. It is mentioned that the positive gain error is 0.5% of FSR. It can be translated to 50mV if the full scale rating is 10V. In the datasheet this parameter is hyper-linked to the note 3 given under table 1. In note 3 it is mentioned that "specifications before calibration. Channel system calibration reduces these errors to the order of the noise".

 

Can I assume that using system calibration mode along with a precise +10V input, this ADC is able to reduce the Positive gain error to an extend of <0.01%.

 

 

Thanks,

Jebas.

Outcomes