AnsweredAssumed Answered

are there options for a single channel SDR chip?

Question asked by pharbour on Jan 6, 2014
Latest reply on Mar 3, 2014 by Vigneshap

Hello,

 

Is there a part similar in architecture to the AD9361 that supports a single RF channel versus the two channel capability of the AD9361?  There is an interest in a single channel SDR (1 TX, 1 RX channel; 3 GHz RF coverage; 20MHz modulation BW).  The WiMax Transceiver chips (AD935x) are interesting, but they are targeted to 3G RF only.

 

 

Thanks,

 

Pete

Outcomes