AnsweredAssumed Answered

Cannot get my ADF4002 to count

Question asked by theadrian on Jan 3, 2014
Latest reply on Jan 5, 2014 by theadrian

I am trying to build a local oscillator synthesizer around an ADF4002.

 

For testing purposes I am driving the serial interface from a Bus Pirate. I seem to be able to send commands to the latches successfully. I can program MUXOUT to DGND, DVDD or SDOUT. when programmed to SDOUT the output matches the input, advanced by 1 clock period.

 

The CP output remains high impedance. When I program MUXOUT to the N or R divider output the result is a logic low with no hint of anything counting. I am stumped at the moment. I am thinking that I may not be understanding the correct protocol. The datasheet makes mention of an 'internal reset pulse'; I am wondering if that is what is stopping the counters. I believe the commands I am sending are as follows:

 

000010010000000011100011

000010010000000011100010

000000000000010010011100

000000000010010100000001

 

AVDD and DVDD are 3V, charge pump is 5V. My FRF is 4.915 MHz and FREF is 38.88 MHz. FRF is AC coupled; FREF is DC driven from 3V CMOS 74AC1G04 inverter.

 

Any suggestions as to what might be wrong would be greatly appreciated. Thanks.

Outcomes