AnsweredAssumed Answered

AD-FMCJESDADC1-EBZ with ZC706 gives SDK jtag error

Question asked by Muhammet on Dec 31, 2013
Latest reply on Jan 20, 2014 by Muhammet

Hi,

 

I want to use AD-FMCJESDADC1-EBZ with ZC706. I imported reference project to SDK.  When I try to program device via SDK, I got the sdk_error which is attached.  When the FMC device is connected to the ZC706 board, it is added to the jtag chain automatically.When i disconnected the AD-FMCJESDADC1-EBZ from the zc706 board, SDK can program the device without error. I dont want the AD-FMCJESDADC1-EBZ to be in the jtag chain.

How can i solve this problem?

 

Thanks in advance,

 

Muhammet ÖZGÜR

Attachments

Outcomes