AnsweredAssumed Answered

FMCOMMS2 Zynq Zedbaord image is missing

Question asked by DanMa on Dec 25, 2013
Latest reply on Jan 3, 2014 by rgetz

Dear All,

 

First let me wish a Merry Christmas to all of you.

 

We wanted to try the linux demo IIOscope. Therefore we downloaded the image from the following link

http://wiki.analog.com/resources/tools-software/linux-software/zynq_images

 

File name is Zynq_image_8gb_2013_12_12 .... ( see Zynq_image.jpg )

then after spending sometime creating an SD card we ended up with this ( see SD-card.jpg).

This could not run on our Zedboard FMCOMMS2 but run on our FMCOMMS1 board. Checking more in detail, the readme.txt dates back to April ( April fool in December ? Is that climate change ).

README: Release April 18th 2013

This release supports following targets.

zynq-zc702-adv7511-xcomm
zynq-zc706-adv7511-ad9250-fmc-250ebz
zynq-zc706-adv7511-xcomm
zynq-zed-adv7511-pmod-ad1-da1
zynq-zed-adv7511-xcomm

Copy target/BOOT.BIN and target/devicetree.dtb to the
root of the BOOT FAT32 partition.
The Linux kernel uImage is the same for all targets.

 

On the link above much more images are listed:

  • ZC702 & the ADV7511

  • ZC702, ADV7511 and the AD-FMComms1-EBZ board

  • ZC702, ADV7511 and the AD-FMComms2-EBZ / AD-FMComms3-EBZ (AD9361) board

  • ZC706 & the ADV7511

  • ZC706, ADV7511, AD-FMComms2-EBZ / AD-FMComms3-EBZ (AD9361)

  • ZC706, ADV7511 and the AD-FMComms1-EBZ board

  • Zed board & the ADV7511

  • Zed board and the AD-FMComms1-EBZ board

  • Zed board and the AD-FMComms2-EBZ / AD-FMComms3-EBZ (AD9361) board

  • Zed board and the AD-FMCMOTCON1-EBZ board

  • Zed board and the FMC-IMAGEON board

So I guess Santa needs to update the image may be he was too busy.

 

Best regards,

Dan

Attachments

Outcomes