AnsweredAssumed Answered

ADV7619 output the even pixels and the odd pixels

Question asked by 宁喜峰 on Dec 20, 2013
Latest reply on Dec 20, 2013 by GuenterL

dear all:

I use the ADV7619 for video receiver,and output the video to DSP.

input formats are 2560x1600 @60Hz  and 3840x2160@30Hz

I saw the ADV7619 spec and I found output TTL 48-bit pixel interface :

the output on the pixel bus consists of two 24-bit buses running at up to 150 MHz: one bus contains the even pixels, and the other bus contains the odd pixels.

p0-p23 -----even pixels is 1,3,5,7,9......;p24-p47 odd pixels.0,2,4,6,8.......

I don't want this mode

if input format is 2560x1600 @60Hz

i need that  p0-p23 are output  0,1,2,3,-----1279  and p24-p47 are output 1280,1281,1282------2559,

How should I set up?

 


Outcomes