AnsweredAssumed Answered

Standalone Flash Programmer

Question asked by jansen on Dec 17, 2013
Latest reply on Dec 19, 2013 by DavidS

I'm attempting to use the SAFP and it has worked twice, but usually fails.  I'm using the example VBScript changed for my files.

 

I have VisualDSP++ 5.070 and am looking to update the program on a small number of third-party devices using SAFP.  To test my setup, I'm reprogramming some devices we have with files built using VisualDSP++ 4.5.

 

I used the configurator to create the .ini file (attached).  Running the test in the configurator passes fine.

Running the script seems to work fine at first.  I get one question when loading the driver.  'built for 0.3 silicon into a 0.5 silicon target'.  I say Yes and it continues.  I've never had this cause problems.  After I click OK in the 'Load the LDR...' file popup I get the error.  The error is 'Could not load file, load will not complete', code '80020009'.

 

The machine being used is an old laptop running WinXP.  Its a bit on the slow side.

 

Any help would be great!

Thanks!

Attachments

Outcomes