AnsweredAssumed Answered

Running EDID Editor in AVES

Question asked by ggottawa on Dec 16, 2013
Latest reply on Dec 19, 2013 by ggottawa

I currently have an evaluation board: EVAL–ADV7619-7511P.

 

For the analysis of ADV7619, I want to analyze its EDID with "EDID Editor" which is included in AVES2 2.05.125.

By the way, I have a problem with running "EDID Editor".

 

First, “AVES2 2.05.125” is open. Then, EDID is run from the main menu, & “Save As” is executed.  

When, I executed the program, the EDID is saved as the name I have specified. Note that its extension is dat. 

Then, the message is “Unable to start EDID editor: The system cannot find the file specified”.

 

 

The, the following is what I have noticed.

In the setting of the main menu, the path of the EDID Editor is set to “C:\Program Files (x86)\Analog Devices\AVES2\EEdit.exe”. 

When I checked this path, EEditor.exe was not in that directory.

 

Is it necessary to download EEditor.exe separately in addition to AVES2?

Outcomes