AnsweredAssumed Answered

ADV7511 and ADV7612 with WUXGA

Question asked by dan73 on Dec 12, 2013
Latest reply on Jan 10, 2014 by mattp

Hi

 

we would like to use those two chips as DVI input and output with UXGA (reduced blanking). Is this mode supported (154MHz)?

is this mode supported with two independent DVI inputs as well?

Is the advertised bandwith of 225MHz the limiting factor?

Example 154MHz for UXGA on input 1 and 25.175MHz for VGA on input 2 would work?

 

Are royalties due when using those chips with DVI or HDMI connectors ?

 

best regards

 

Dan

Outcomes