AnsweredAssumed Answered

Aliases between hierarchy boards?

Question asked by PeterTheRed on Dec 10, 2013
Latest reply on Dec 12, 2013 by PeterTheRed

I'd like to simplify my project and reduce processing load by using a single DC source for (each of) logic high and logic low.  It would seem a simple thing to create an alias 'send' from each DC source, and paste copies of the alias 'receive' wherever needed.  However, I can't seem to paste an alias receive into a different hierarchy board than its associated send.  Likewise, if the send is on the main page, I can't paste the recieve into a hierarchy board.  Is this by design?  I've observed this in both 3.8 and 3.9 beta.  I s'pose I could create additional inputs to each hierarchy board that needs these logic levels and keep all the aliases on the main page, but that adds to the clutter...  Thoughts?  Thanks!

Outcomes