AnsweredAssumed Answered

About SPI_MISO pin of ADV7630

Question asked by Kikka on Dec 2, 2013
Latest reply on Dec 4, 2013 by Kikka

Hello.

 

Let me confirm about SPI_MISO pin of ADV7630.

 

UG-399 says the following.

 

>SPI_MISO tied to REG_3P3V. Causes HPA to be low when cable is plugged into chassis-powered-down ADV7630

 

Currently, SPI_MISO tied to REG_3P3V through 10k ohm resistor.

 

Would 10k ohm resistor cause any problems?

Should I change it to 0k ohm resistor from 10k ohm resistor?

 

Best regards.

Kikka

Outcomes