AnsweredAssumed Answered

A quick question about the EVAL-CED1Z

Question asked by evalon on Nov 28, 2013
Latest reply on Dec 15, 2013 by evalon

Hello Analog Devices,

 

I'm considering buying an EVAL-CED1Z to use mainly with the AD7760 (2.5 MHz), however, if there is an ADC with a (somewhat) higher sample rate that can be used with the same evaluation board that would be very interesting. I'm looking for sample rates of at least 10 MHz at 20 - 24 bits resolution.

 

Might one of you know if the EVAL-CED1Z can be used with a higher sample rate ADC than the AD7760's 2.5 MHz?

 

Thanks for reading and hopefully replying

 

Jesper Mønsted

Outcomes