AnsweredAssumed Answered

ADSP 21065L SDRAM Controller problem

Question asked by Clementina on Jun 16, 2010
Latest reply on Jun 21, 2010 by vishwanath

Hi,

 

I have this unworking scenario on my board with a adsp as in object. In few words the instructions are abnormally modified when placed in external sdram segment.

 

I attached two files in which you can see, in mixed mode, how the code is disassembled.

 

In "int_mem.txt" file the cut/pasted code is ok and I can read/write in the external sdram while in "ext_mem.txt" one the code has been placed in pm external memory but it doesn't work properly !

 

Assuming that the board has been correctly designed, how can I test the DSP to be sure that I have to replace it ?

 

 

 

 

Note:

 

seg_pmco { TYPE(PM RAM) START(0x00008200) END(0x000097ff) WIDTH(48) }

pm_sdram { TYPE(PM RAM) START(0x20000) END(0x2fffe) WIDTH(32)  }

 

// SDRAM Controller Register

ustat1 = 0xA87298FF;

DM(IOCTL) = ustat1;
NOP;

 

Messaggio modificato da Clementina

Attachments

Outcomes