AnsweredAssumed Answered

MISRA rule error: No space to do runtime checking on rules 17.1, 17.2 and 17.3 (suppress checking! )

Question asked by sujan5614 on Nov 18, 2013
Latest reply on Nov 21, 2013 by sujan5614

Hello,

 

We are using ADSP-BF548 in one of our project.

Ez Kit Lite: ADSP BF548 EzKIt lite rev 1.2

IDE version used: CCES v1.0.2

 

For Hardware testing, a simple test code is implemented which tests the basic interfaces UART0, SPI1, SPORT2 and SPORT3. A simple loopback is performed on the interfaces over a terminal. After several cycles of loopback testing we are getting the following message on the terminal:

 

    "No space to do runtime checking on rules 17.1, 17.2 and 17.3 (suppress checking!)" and the processor hangs.

 

I went through the thread http://ez.analog.com/message/44753#44753, and verified that my MISRA-C rule checking is disabled.(in properties -> CrossCore Blackfin C/C++ Compiler -> MISRA-C -> "Enable MISRA-C conformance checking" is unchecked)

 

Please suggest on how to disable the MISRA rule check.

 

Regards

Sujan.

Outcomes