AnsweredAssumed Answered

Driving AD7663(16 bit ADC) using AD8421(Instrumentation Amp)

Question asked by jebaspaul on Nov 18, 2013
Latest reply on Nov 18, 2013 by KarenNE

Hi,

 

I am designing a 16 bit 24 channel DAS. The input is differential +/-10V. AD8421 is used to remove the common mode signal. The output of AD8421 is single ended Bipolar +/-10V. Signal at the input of IA is varied at 50Khz. The input is DC which varies from +/-10V across channels. So effectively the worst case load is a 50Khz square wave with 20V p-p.

My intention is to use the instrumentation amplifier AD8421 as a driver for ADC.So, that I can avoid an additional driver in the signal line.  The datasheet of AD7663 suggest to use a RF filter with R(=15ohm) and C(=2.7nF) in between driver and ADC.

 

Can I use AD8421 to drive AD7663 with & without the above mentioned RF filter.

Please give your suggestions.

 

 

Thanks,

Jebas.

Outcomes