AnsweredAssumed Answered

AD9959 Eval Board and 64-bit Windows

Question asked by DaveZ on Nov 14, 2013
Latest reply on Jul 29, 2014 by CSeck

I have been using the AD9959 Evaluation Board to create signals for an FM-CW radar application.  I have written my own software to control the board via the USB port, following the example of your Evaluation Software (using C#, MS Visual Studio 2010).  This works successfully on Windows XP.  I have now modified my code to run under 64-bit Windows (7 and 8).  This, too, works successfully -- but only after the Evaluation Board has had its firmware uploaded using the AD9958/9959 Firmware Loader device driver provided with the Evaluation Software, which only runs on 32-bit Windows.

 

Is it possible to obtain the firmware code that is uploaded by the Evaluation Software so that I can load it onto the Evaluation Board from my 64-bit program?   Any suggestions as to the best way to do this upload would be greatly appreciated.  Thanks.

Outcomes