AnsweredAssumed Answered

BF506F - SPORT1 (ACM module) Problem

Question asked by srelee on Jun 14, 2010
Latest reply on Mar 15, 2011 by WassimB

Hello,

 

I am working on internal ADC of BF506F , I programmed it through ACM module . But when I activate SPORT1 module to collect data of an ADC, the data in the RX buffer of SPORT1 is displaying as '0x00000000' . But ADC OUTA pins are displaying the results. Please help me out in getting the data in SPORT1 Buffer.

 

The input used is 'DC cuurent of 1 V from function generator.'

 

The code sample is attached.

 

Thanks,

Sree

Attachments

Outcomes