AnsweredAssumed Answered

Is it possible to run and use 'Chipscope analyzer' with .ace image running on ML605

Question asked by FArid on Nov 11, 2013
Latest reply on Nov 15, 2013 by rejeesh

Hi

 

I'm using reference image (.ace) file for AD-FMCOMMS1 running on ML-605 (revE).

I wonder how to run Chiscope anlyzer when this reference design is running on ML605 and AD-FMCOMMS1.

When I try to run it, it shows successful connection to server:

 

COMMAND: open_cable

INFO: Attempting to connect to an existing server.

INFO: Successfully opened connection to server: 192.168.2.2:1234 (192.168.2.2/192.168.2.2)

 

however searching for cable is taking like forever and shows this:

 

WARNING: Server connected but not responding after 60 seconds.

The server may be in use by another ChipScope client configuring a large device or

the port may already be in use by a non-ChipScope server.

You may want to exit the program and try a different port.

 

I'm using HyperTerminal to have the prompt to device. However, even when I close it the same thing appears. What part I'm doing wrong?

 

FArid

Outcomes