AnsweredAssumed Answered

How to use HTTP_Server in BF536?

Question asked by danilliu on Jun 10, 2010
Latest reply on Jun 28, 2010 by CraigG

Hi!

 

How can I port the Web server example in the VisualDSP++ to my BF536 board? the example is originally port for BF537.

 

I have refered the EE-315 document to  change the PHY driver for my PHY chip;

 

then I open the Web server example project group  according to the document "LWIP User GUIDE". Changed the Target\Processor to ADSP-BF536 of the two project in the project grope.    As there are 16M SDRAM in my board, I set the Extended Memory value accordingly.

 

I also added a macro "__ADSPBF537__" in the Preprocessor definition to avoid compile error.

 

 

The project group can be compiled with no error. But it can't run correct  -after I build project(F7), it loaded to the RAM and RUNING automatically  - I have not press F5 key yet! and there's no message printed out.

 

Is there any thing wrong ?

 

thanks for any help.

 

danilliu

Outcomes