AnsweredAssumed Answered

BF60x DMC - not in use

Question asked by KevinL Employee on Oct 30, 2013
Latest reply on Nov 11, 2013 by Mitesh

Hello,

I'm looking for a comprehensive checklist of things that must be done when the BF60x DMC is NOT used, such as pin handling and required register settings. Is such a list available?

 

Also, it is noted in BF60x Hardware Reference (Rev 0.5), on page 11-46:

1. Bits 6, 7, 24, and 26 of the DMC_PHY_CTL3 register all need to be set to 1.

2. DMC_DLLCTL register needs to be set to 0x54B. This keeps the default reset values and programs DATACYC to a value of 5.

If the DMC is not in use, are these register settings required? If not, are the reset values of these two registers sufficient?

 

thank you,

Kevin L.

Outcomes