AnsweredAssumed Answered

ADuC7060 Serial Download

Question asked by KevinM on Oct 25, 2013
Latest reply on Oct 29, 2013 by KevinM

Hi,

 

I've built a prototype using the ADuC7060 and ADM3202 for RS232 communication. I copied the evaluation circuits, but it doesn't work.  The WSD application just sits there waiting for the response from the controller.  I need some help understanding what is supposed to be happening on the microcontroller when I pull the pull NTRST/BM pin low. I'm also wondering if there is a way to tell if the micro is functioning properly aside from knowing I have power at the correct pins.

 

Attached is the portion if the schematic with the ADuC7060 and ADM3202.

 

Any help would be appreciated.

 

 

 

 

Kevin Mason

Managing Partner

Apogee Information Technology LLP

kmason@apogeeinfotech.com

 

 

Outcomes