AnsweredAssumed Answered

ADV7611 - QVGA input

Question asked by altrchris on Oct 25, 2013
Latest reply on Nov 18, 2013 by mattp

 

Hello,

 

I'm newbie in this field.

I need to drive a QVGA LCD display (320x240@60Hz) like this one : http://www.data-modul.com/tl_files/dm/data/specification_CA10013.pdf and the HDMI signal which  comes from a cpu is compliant HDMI 1.4.

My question is simple : can I drive the QVGA display directly by the ADV7611 or do I need another video processor to convert the signals coming from the ADV7611 into what the display is expected ?

 

Thanks

Regards

Outcomes