AnsweredAssumed Answered

Are there application notes/schematics showing the AD8000's configured as an instrumentation amplifier?

Question asked by Kyle.Ogden on Oct 23, 2013
Latest reply on Oct 25, 2013 by Kyle.Ogden

Hello,


I need to build an ultra-high speed instrumentation amplifier for an ultra-wideband radar I am building.  Are there application notes or schematics to use the AD8000, AD8003, or the AD8009 configured as an instrumentation amp? I need an instrumentation amplifier that can handle frequencies up to 1.5 GHz.


Thank you,

Kyle Ogden

Outcomes