AnsweredAssumed Answered

Error when build kernel to support MCAPI

Question asked by pengpeng on Oct 23, 2013
Latest reply on Oct 28, 2013 by Aaronwu

Hi Aaronwu,

 

Thanks for your suggestions, I am able to use svn to retrieve all the packages and build my own kernel uImage (bf609 default). Now I am exploring the multicore communication feature (after make mrproper in linux/linux-kernel and make clean in adi-buildroot-code folder, seperately). Then,

 

Following exactly according to: http://blackfin.uclinux.org/doku.php?id=test_icc, I have reached the stage:

 

make packages/icc_utils_only

 

saying that no rule to make it. I checked that folder, there is no makefile. So I was wondering where could it be?

 

Then I skipped this and followed:

http://blackfin.uclinux.org/doku.php?id=test_mcapi

to get a kernel image which supports MCAPI.

 

Then I got error when:

 

make libmcapi

 

under adi-buildroot-code directory. The error message and log files are listed as below:

 

configure: WARNING: unrecognized options: --disable-gtk-doc, --disable-nls, --disable-ipv6

configure: error: in `/home/y/adi-buildroot-code/output/build/libmcapi-668/libmcapi-2.0':

configure: error: C compiler cannot create executables

See `config.log' for more details

make: *** [/home/y/adi-buildroot-code/output/build/libmcapi-668/.stamp_configured] Error 7

 

 

Any ideas? Thanks,

Attachments

Outcomes