rbrennan

ADF4360-x software

Discussion created by rbrennan Employee on Oct 22, 2013
Latest reply on Sep 3, 2015 by rbrennan

The latest ADF4360-x software is attached. This is compatible with all the ADF4360 family.

 

Installation process:

1. Disconnect any evaluation board

2. Download and run the attached installer

3. Click Next/Continue/Finish when asked

4. Connect your evaluation board

5. Windows will detect the evaluation board and install the drivers

6. Run the ADF4360-x software from the desktop or Start Menu

7. The status bar of the software should show that the board is connected. If not, try disconnecting and reconnecting the board.

 

Installer includes USB drivers.

 

  • v4.3.0: Fixed N value rounding error and improved usability.
  • v4.2.0: Housekeeping.
  • v4.1.2: Added 10 ms delay between Control Latch and N Latch when Write All Latches button is used. See page 17 of ADF4360-7 data sheet.

Attachments

Outcomes