AnsweredAssumed Answered

ADXRS649 Calibration Options

Question asked by larosta on Oct 21, 2013
Latest reply on Dec 27, 2013 by NevadaMark
Branched from an earlier discussion

I need to calibrate an instrument that uses the ADXRS649 (+/- 20000 °/s) rate gyro.  This gyro will be used in a rate sensing application and will not be in a closed control loop so we need pretty good accuracy in the calibration scale factors (>= 1% of full scale).  I do not believe the the technique described in the referenced document will provide the accuracy we describe.  My question is, can someone here on the forum suggest a calibration lab here in the US that would be able/willing to calibrate these devices?

Outcomes