AnsweredAssumed Answered

AD-FMCOMMS2-EBZ and ZC702 or ZC706

Question asked by hight77 on Oct 21, 2013
Latest reply on Oct 25, 2013 by mhennerich

We have the ADFMCOMMS2-EBZ (AD9361) dev board and a ZC702 platform.  I built the demo image provided by AD for the ZC702(zynq_image_8gb_2013_10_1.img.xz)

 

To my surprise there is a directory for the ZC702 and AD9361 as well, so I moved the boot files to the root directory and tried it out.  It boots just fine, but I get the following error...

 

ERROR: could not get clock /fpga-axi@0/cf-ad9361-dds-core-lpc@79024000:sampl_clk(0)

 

Of course, the GUI does not show the AD9361.

 

I do know that at least the SPI port to the AD9361 is working since I have verified it with a custom design.  I am also able to enable and control the user clock output with the custom design.  FYI, the custom design is running on a Spartan-6 dev board with the AD-FMCOMMS2-EBZ.

 

Has anyone else tried the demo on a ZC702?  Or has anyone tried the demo with either the ZED or ZC706?

 

I would like to know if it really works before we drop $2500 on a ZC706 (we can't find ZEDs in stock).

Outcomes