AnsweredAssumed Answered

ADV7619 - resolution capability

Question asked by ggottawa on Oct 16, 2013
Latest reply on Oct 17, 2013 by ggottawa

Hi, I think ADV7619 is a potential candidate for my project.

I have a few questions on ADV7619.

 

a. Spec shows that the chip has two HDMI inputs. Can each HDMI input handle only up to 1080p? Or can each input process as high as 3840 x 2160 resolutions@30Hz?

b. Spec says, “Fast switching between both HDMI input ports in less than 1 sec”. Does it mean that one port will be used at a time? 

c. Does Analog Devices produce an HDMI-receiver which is capable of up to 4k x 2k @30Hz while it has only one channel instead of two like ADV7619?

 

Thank you.

Outcomes