AnsweredAssumed Answered

PinOut to accelerometer ADXL312 map

Question asked by gundamned on Oct 15, 2013
Latest reply on Oct 21, 2013 by venkat

Hello all,

 

i have an UG-209 evaluation board, with a satellite board with the ADXL312 accelerometer. I would like to attach this satellite board with another MCU, but I need to know which are the 4 pins for SPI communication on the satellite board.

 

So my question is: is there an explanation on which pin of the ISEB 20-pin blue connector the ADXL312 pins are connected to?

For example, where the CS pin of the ADXL312 (pin 6) is on the blue connector, which pin?

 

Greetings,

Mark

Outcomes