AnsweredAssumed Answered

adi_core_b_enable issue

Question asked by MikeSmithCanada on May 29, 2010
Latest reply on Jun 2, 2010 by CraigG

Am trying to move some working 533 code over to one core of 561

 

I build a two core 561 project -- with one of the core's running idle -- then added the code from the working project and got it to compile.

 

I was under the impression that the second core would not start until the code -- adi_core_b_enable -- was run from core A:

However VDSP seems to allow that core-B to run by itself -- which means that when I try to download both executables into their represtative cores -- VDSP says that it can't stop the other core, the system wants to disconnect and the crashing everything

 

DO I ned to find a way to set bit 5 of the SICA_SYCR via VDSP?

 

Message was edited by: Michael Smith

Outcomes